StringFunctions.Replace function

Replaces all occurrences of string_exp2 in string_exp1 with string_exp3

Format

SQL Format:

Replace( string_exp1, string_exp2, string_exp3 )

ODBC Format:

{{ FN Replace( string_exp1, string_exp2, string_exp3 ) }}

Remarks

Returns a string expression that reads like string_exp1 except that any occurrences of string_exp2 therein will have been replaced by string_exp3.

string_exp1 can be any string expression.

string_exp2 can be any string expression.

string_exp3 can be any string expression.

Example:

Replace( 'I drove to the market', 'drove', 'cycled' )

{FN Replace( 'I drove to the market', 'drove', 'cycled' )}

returns the string expression 'I cycled to the market'.


Disclaimer

Geo SCADA Expert 2021